Posted on November 2, 2021
Victaulic Tools for AutoCAD® won gold in the Consulting-Specifying Engineer’s 2021 Product of the Year (POY) program in the Software: Design, Modeling, Monitoring category. The contest highlights new products in the HVAC, fire safety, electrical, and plumbing systems engineering markets. Victaulic Tools for AutoCAD is a free tool that provides AutoCAD® users the same classic routing features and drawing productivity gains that were previously only available in the Victaulic Tools for Revit® platform. The VTFA add-on provides toolsets engineered for civil, industrial, plant or mechanical projects, and includes features to simplify pipe routing, procurement, and exporting bills of materials.
VTFA gives contractors and engineers a free tool that not only streamlines the design phase but also helps expedite the fabrication stage of a project. This AutoCAD® add-in bridges the gap between design and fabrication by providing the platform and the tools necessary for contractors to seamlessly route piping, generate accurate spools, and manage projects faster from the start. Victaulic’s dedication to providing industry-leading software is driving growth by enhancing routing efficiencies and delivering cost certainty throughout the project lifecycle.
In 2019, Victaulic won Gold and Bronze CSE Product of the Year awards for the FireLock™ IGS™ Installation-Ready™ Style V9 Sprinkler Coupling and Grooved Sprinkler and the QuickVic™ SD Installation-Ready™ System, respectively.
Check out Consulting-Specifying Engineer for more details.