Victaulic in the Vineyard: Mechanically Joining HDPE Saves Time & Money

vineyard with ripe grapes in countryside at sunset

Victaulic in the Vineyard: Mechanically Joining HDPE Saves Time & Money

Posted on June 28, 2018

Victaulic’s System Solution for High-Density Polyethylene (HDPE) proved to be key in the ahead-of-schedule completion of buried heating and cooling water piping at the Four Seasons’ new Residences at Napa Valley. Not your everyday hotel, the Calistoga, California property includes individual farmhouse-style villas designed to maximize the experience of California wine country.

 

buried insulated and non-insulated heating and cooling water distribution piping joined with Victaulic style 905 couplings for hdpe pipe.The Blueprint

The multiple-building layout of the Residences at Napa Valley property required underground HDPE lines for cooling and heating water distribution, which run from a central utility plant to each residence throughout the property.  Both insulated and non-insulated pipes were used in horizontal and vertical orientations for the 5,000 foot HDPE portion of the project and Victaulic® solutions, including fittings, couplings, and mechanical tees, were installed throughout the project in 2, 4, 6, and 8-inch sizes.

 

Style 905 couplings joining HDPE pipes.The Install

Contractor Greenberry Industrial of Vacaville, California chose to use Victaulic’s products based on time and cost savings. Without Victaulic’s HDPE technology, Greenberry would have added over 75% more labor for the installation of the HDPE systems. Less labor resulted in cost savings and a shortened project timeline. As an added bonus, Greenberry retained the ability to make pipe length changes onsite and enjoyed the confidence that comes with Victaulic’s “bolt pad-to-bolt pad” visual confirmation of correct installation. With less labor needed, Greenberry was able to reallocate workers to advance other portions of the project, allowing for reburial of the water lines and the pouring of building slabs ahead of schedule.

 

Victaulic’s technology makes HDPE pipe extremely easy to work with. The pipe can be joined very quickly and with minimal labor, resulting in huge savings. We are excited for future projects where we can use HDPE and Victaulic.

Jared Goodreau
Construction Manager, Greenberry Industrial

 

The Verdict

More design engineers and contractors are turning to HDPE for major piping projects. By using the simple, durable, and designed-to-be-buried Victaulic system, contractors can bypass the limitations of fusion and move forward on schedule regardless of weather. Without Victaulic’s solutions, installation of the Four Seasons project’s water distribution system would have consumed significantly more time and money. The demonstrated superiority of Victaulic’s mechanical solutions for HDPE on this job proves that Victaulic’s System Solution for HDPE Pipe is THE joining system for all “four” seasons.

 

To learn more about Victaulic’s System Solution for HDPE Pipe performance, click here.

Related posts

Victaulic Adds Plug Valve to StrengThin™ Piping System, Updates Grooved Coupling Design

Victaulic Adds Plug Valve to StrengThin™ Piping System, Updates Grooved Coupling Design

This innovative piping system solution allows for faster pipe fabrication & field installation, improves safety & reduces project costs.

Victaulic Attends the AHR Expo with New Products & Technologies

Victaulic Attends the AHR Expo with New Products & Technologies

Learn about our new grooved pipe joining products & technologies at the 2015 AHR Expo in Chicago.

Release of Compact, Precise Hydronic Balancing Valve from IMI TA

Release of Compact, Precise Hydronic Balancing Valve from IMI TA

The TA Series 7CP advances hydronic balancing with its compact size & ability to engineer high performance systems.