Faster, Safer, More Accurate Approach to Pipe Fabrication

Victaulic RG5200i Intelligent Roll Grooving Tool Close Up

Faster, Safer, More Accurate Approach to Pipe Fabrication

Posted on January 17, 2017

New High-tech Solution to Pipe Fabrication Challenges

Improves safety, accuracy, time and productivity — while reducing costs for fabricators.

Fabricators who prepare piping for application in new construction or renovation projects face numerous challenges. These range from the costly problems of unpredictable environmental factors, human error and integrity of the piping, to the very real, crucial issues of worker safety. A new, fully automated, computerized advanced grooving device has been introduced that drastically reduces the possibility of measurement errors, while making the fabricators’ workplace a markedly safer and more productive environment.

The new technology comes in the form of the “intelligent” RG5200i Roll Grooving Tool from Victaulic, the world’s originator and leader in the development and production of mechanical pipe joining solutions. Company officials and end-users report that the device is changing the system of pipe fabrication and, ultimately, ushers in the era of an entirely new and highly exacting method of pipe grooving.

In development for years yet formally introduced in August 2016 by Victaulic, the RG5200i Roll Grooving Tool represents a significant advancement in enhanced workplace safety, reduced man-hours, reliability, cost-effectiveness, and precision pipe grooving.

Safety

Matthew Puzio, Senior Electrical Engineer at Victaulic, notes that the new technology answers calls for increased worker safety, as much as it does for creating a more streamlined, efficient workplace. “Today, machine tool builders focus on using safety devices to drive efficiency in the manufacturing environment.

“Traditional grooving is a very manual process, where the operator has influence over groove quality and the way the joint is formed,” Mr. Puzio explains. “With the RG5200i Roll Grooving Tool, you get the right groove every time. Quality control is built into the system.”

Since Victaulic is already world renowned among fabricators and engineers as a leader in mechanical pipe joining technology that largely eliminates the need for potentially hazardous welding, the company saw the need for an ‘intelligent’ grooving tool that went several steps beyond safety, reliability and efficiency.

Victaulic engineers envisioned a grooving tool that would put worker safety at the forefront — while revolutionizing the way fabricators perform their often complicated and time-consuming trade. With the right technology, Victaulic engineers felt fabricators could work to more exacting standards, reduce man-hours, cut costs, improve the integrity of the grooved pipe, and do it all in a safer work environment. The RG5200i Roll Grooving Tool has achieved all of the aforementioned goals. The tool succeeds in fully automating the grooving process — while integrating cutting-edge proprietary computer software accompanied by laser technology to yield precision results.

“The technology available to us now, compared to even five years ago, has been a big player in permitting us to make some of these components,” Mr. Puzio explains. “That is what spurred the idea to create the smart tool.” When the Victaulic team approached designing the RG5200i, the focus was on lean fabrication, improving how operators use the tool, as well as a renewed concentration on ergonomics.

Paramount within the tool’s design are its built-in safety features. The RG5200i Roll Grooving Tool is designed with a proximity “no-go” zone surrounding the perimeter of the machine; that is, should anyone enter the safety zone, sensors detect movement and the operation is automatically halted. “In fabrication shops, it’s safety first,” insists Mr. Puzio.

This technological enhancement avoids accidental start-ups, a critical safety feature. The RG5200i Roll Grooving Tool virtually eliminates costly shut-downs, keeping the work on schedule. In addition, operators work from a remote pedestal located away from the actual grooving mechanism, adding another element of worker safety.

Reliability

Before the advent of the RG5200i Roll Grooving Tool, fabricators using traditional pipe end preparation tools had to rely on their machine operators to execute and analyze the correct groove. “Some fabricators were concerned that there wasn’t enough shop staff to handle it,” Mr. Puzio explains. They’d be reluctant to dedicate a welder to a grooving tool, so they would often have to opt for a less experienced employee to expedite the job. “But [worker training and experience] concerns could arise,” Mr. Puzio acknowledges. The RG5200i Roll Grooving Tool renders that issue moot. Since it’s automated, “it allows anyone to use it,” he explains. “This builds confidence in the user, be it a newcomer or a 20-year veteran.” Additionally, the tool builds the customer’s confidence that they are creating an in-spec groove while reducing variability in the manufacturing process.

Designed to groove carbon steel pipe in diameters from four inches to sixty inches, the RG5200i Roll Grooving Tool takes the guesswork out of pipe grooving because it converts much of the effort from a manual to an automatic process. Thanks to laser technology, pipes are grooved to exact specifications, with a record of every pipe groove stored in a database.

“Pipes are made to different specs; as such the operator needs to consistently check the grooving parameters and adjust as needed,” Mr. Puzio adds. “There are also flow control valves that need to be adjusted. Essentially the machine setup operator needs to focus on the machine to get it to groove properly.”

The RG5200i Roll Grooving Tool “reads all of these factors automatically; it determines whether to groove faster, deeper, etc.,” Mr. Puzio continues. “It achieves all of this without the need to adjust it manually.” This includes the device’s depth stop, which is located on top of the machine. Fabricators “used to have to get a ladder to make adjustments on the tool,” Mr. Puzio points out. “Our new tool automatically reads the pipe and adjusts groove speed and depth, saving time on initial set up or pipe size changes.”

Traceability

Among the chief attributes of the RG5200i Roll Grooving Tool is its focus on data acquisition technology. “While the tool is grooving it’s reading all of the dimensions,” Mr. Puzio explains. “When it hits the diameter target, all numbers are read and recorded in our system.” This amounts to “full traceability” of every aspect of every fabrication job, he notes, which represents a major step forward in fabrication technology.

Connectivity

Inherent in the tool’s design is its internet connectivity, a vital resource for troubleshooting issues such as pipe alignment. The 5200i uses internet connectivity for software updates, data extraction, and trouble shooting if necessary. The technology also provides a live stream of shared information. “If there is an application issue, we can be there with the customer by connecting via IP camera,” Mr. Puzio explains. Victaulic engineers can view exactly what the customer sees — in real time. “It’s smart technology — very state of the art,” he says. “it’s also a strong service aspect for our customers.”

The intuitive nature of the RG5200i Roll Grooving Tool stems in large part from its reliance on patented grooving process and proprietary software, developed by Victaulic specifically for the new tool.

Ease of Use

In addition to safety, accuracy and reliability, chief among the tool’s advantages is its focus on ease of function and operator use. Ergonomically, it is a vast improvement over manual grooving machines. Operators of older machines had to manually work a foot pedal for hours on end, a tedious aspect of the job. With the new automatic tool, operators can stand by and observe the grooving process, without succumbing to fatigue — further reducing the possibility of a workplace mishap. “Now the whole process is much more comfortable for the operator, and it drastically reduces risk,” Mr. Puzio states. While operators still need to monitor the process, the automated grooving tool makes the entire procedure easier and less physically demanding overall.

Customer Feedback

Since its formal introduction, the RG5200i Roll Grooving Tool has already received accolades from customers. Dave Liggett, Mechanical Fabrication Shop Manager at S.A. Communale, has worked in the industry for a 25 years; he’s been relying on Victaulic grooving tools the entire time. The RG5200i has already had an impact on his business.

“With the introduction of the RG5200i to our facility it gives us the ability to tell our customers that that groove is certified to spec,” Mr. Liggett explains, “but without having to make adjustments between size changes, it’s quicker because you hit the button, you go to six; you hit the button you go to four. It’s just a button instead of measuring and setting depth and trial and error. There’s no more trial and error. So that’s been the biggest benefit.”

The new machine is also well received by Mr. Liggett’s colleagues, he says. “The personnel like it; they like being able to hit the button and let the machine do all the thinking.

“To be able to call and say, ‘Hey this is the error code’ or ‘this is what we’re getting,’ they [Victaulic support] log in from wherever they’re at and they can see the problems, or at least address it and say, ‘hey try this or change this,’” Mr. Liggett explains. “Definitely the benefit is the support — to be able to call whenever and get back online and grooving again.”

“If they have a project, I make sure they enter that into the log so we know which groove is which. We now have the technology, we have the tool, and we can keep the log information in our back pocket in case something ever happens.”

Victaulic has received high marks from companies like Ferguson/FEI, the number-one purveyor of wholesale commercial and residential plumbing supplies in the United States, to suppliers and fabricators of all sizes. “The biggest challenge with grooving pipe has to be grooving the pipe to specification required,” explains Jimmy Utz, Fabrication Shop Lead at Ferguson/FEI. “Anyone can take a piece of pipe and put a groove in it. The challenges become, how do you get the ‘a’ dimension, the ‘b’ dimension and the ‘c’ diameter and control the flare. Those are your challenges. We absolutely track every groove that we run through here. We currently check 100% of our ‘c’ diameters; on roll groove pipe we check the first, the 30th and last of every ‘a,’ ‘b,’ ‘c’ and flare. All of that data is then taken into the office, punched into a database, scanned, registered and saved.

Mr. Utz says he is switching to the RG5200i because of the ease of specification and ease of acquiring specification. He also says it gives his team confidence in the accuracy of their grooves and aligns them more strongly as a vendor and distributor with their end customers.

“We have common goals of working together going forward,” he points out, “having a machine that is providing an accurate groove, and at the same time not only providing you with an accurate groove efficiently but also providing you (with) that level of safety that you need in an environment such as this.”

Mr. Puzio of Victaulic sees the new tool as a boon for businesses going forward. “A wide range of companies will be using this tool,” Mr. Puzio predicts. “Usually it’s competitive; two or three fabricators compete with each other, and that’s what drives people to select this tool. Our questions are: How do we focus on quality and give our customers what they want? How do we make our shops more productive? These are our thrusts: to make shops more productive and competitive in their industry. This tool is another component in that mission and trend.

“It’s something we’ve been trying to do for a long time — trying to develop a tool that achieves all of this,” Mr. Puzio concludes. The RG5200i Roll Grooving Tool has exceeded expectations, he adds, and shows all signs of piquing the interest of demanding suppliers and fabricators in the US, and overseas. “It’s going to be big all around for us.”

Related posts

Victaulic Adds Plug Valve to StrengThin™ Piping System, Updates Grooved Coupling Design

Victaulic Adds Plug Valve to StrengThin™ Piping System, Updates Grooved Coupling Design

This innovative piping system solution allows for faster pipe fabrication & field installation, improves safety & reduces project costs.

Victaulic Attends the AHR Expo with New Products & Technologies

Victaulic Attends the AHR Expo with New Products & Technologies

Learn about our new grooved pipe joining products & technologies at the 2015 AHR Expo in Chicago.

Release of Compact, Precise Hydronic Balancing Valve from IMI TA

Release of Compact, Precise Hydronic Balancing Valve from IMI TA

The TA Series 7CP advances hydronic balancing with its compact size & ability to engineer high performance systems.