Installations With Results

QUICKVIC™ SD HVAC CASE STUDY:
COURTYARD MARRIOTT

HOTEL IMPROVEMENTS FOR BETTER GUEST EXPERIENCES

LOCATION:
  • Santo Domingo, Dominican Republic
FACILITY TYPE:
  • Hotel
PROBLEM:
  • Minimize downtime of hot water system
  • Threading and pressing presented mess and hassle
  • Lengthy inspection process with threading
Benefits of QuickVic™ SD
  • Ease and speed of installation
  • Time savings
  • Simplified maintenance
Read On
The Courtyard Marriott in Santo Domingo is a five-story hotel in the center of the city with amenities such as an onsite restaurant, fitness center, business meeting spaces, and much more. The hotel needed to minimize the downtime of the hot water system when retrofitting two large storage tanks, two water heaters, and all of the 2” and smaller pipe systems to avoid interrupting the function of the building. Traditionally, threading would be used in this type of retrofit project, but the Victaulic QuickVic™ SD Installation-Ready™ System was chosen for its speed of installation and reliability. This solution eliminates the mess and hassle of threading and the lengthy inspection process. The contractor was able to visually inspect QuickVic SD for pad-to-pad contact, and patented “Leak-If-Not-Tightened” technology helped ensure a proper connection, offering peace of mind. The customer estimated that QuickVic SD installed up to three times faster than it would have taken to install and inspect a threaded piping system. This equates to time that hotel guests were not without amenities, resulting in savings for everyone involved. Victaulic’s reliable products will earn the Marriott up to 90% time savings on leak repairs they could potentially face with a threaded system. As the most economical and efficient pipe joining solution for small diameter carbon steel pipe, the QuickVic SD Installation-Ready System was the right choice for this facility.
The customer estimated that QuickVic SD installed up to three times faster than it would have taken to install and inspect a threaded piping system. This equates to time that hotel guests were not without amenities, resulting in savings for everyone involved.
SERVICES
Hot Water
PIPE MATERIAL
Schedule 40 Carbon Steel
PIPE SIZE RANGE
½ – 2"/DN15 - DN50
OWNER
Marriott Hotels
CONTRACTOR
Simep Dominicana S.R.L.
ENGINEER/CONSULTANT
Simep Dominicana S.R.L.
DISCOVER HOW QUICKVIC™ SD CAN BENEFIT YOUR NEXT PROJECT
Learn More

CHECK OUT MORE PROJECTS AND CLIENTS THAT HAVE BENEFITTED FROM QUICKVIC SD INSTALLATIONS

APARTMENT BUILDING UPGRADE BENEFITS TENANTS
  • Ease & Speed of Installation
  • Simplified Maintenance
  • Labor Savings
Learn More
UNIVERSITY EXPANDS ITS TEACHING LABS
  • Cost Savings
  • Ease and Speed of Installation
  • Ease of Rework
Learn More
DISCOVER HOW QUICKVIC™ SD CAN BENEFIT YOUR NEXT PROJECT
Learn More